This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQEVSW: Using BQEVSW to confirm EV2400 FW Revision

Part Number: BQEVSW
Other Parts Discussed in Thread: EV2400, BQSTUDIO

Posting for a customer:

Is it possible to confirm the FW revision of an EV2400 using BqEVSW? 

Here is why I ask.  One of the requirements is to identify and document the firmware and its revision of the EV2400.  However it appears that the firmware revision can only de identified with bqStudio or the FW update tool.  Which means additional SW would need to be loaded on the test system that would not be used.  We can do this if it is the only way to get the FW revision but if there is a way to do it with bqEVSW that would be cleaner.

Your insight on FW revision confirmation of the EV2400 is greatly appreciated.