Hello,
My customer looking for isolated DC/DC with the following properties:
- Input power: 10V DC ~ 30V DC (can be less than 10 and higher than 30)
- Output power: 100V DC (+/- 5V)
- Max Output current : 10mA
- Isolated
Hope that someone can advise.
regards,
Shahaf