This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
2 things:
1. Is there any tool (like webench) in which I can easily check/simulate the LM2611A with values that I have put into the circuit?
2. I do not see any easy formula for the calculation of the feedback resistors on the datasheet. Is there any?
Below is the schematic- 12V input and -6V output circuit.
Please suggest me any changes needed in the above circuit.
Thanks & Regards,
Nanjunda M
Hi Zack,
Is there any excel sheet to verify the values?
Could you please provide your feedback on the circuit attached to the above post.
Thanks & Regards,
Nanjunda M