This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: LM5022 Vin pin is out of control

Part Number: LM5022

Customer wants to know the answer to the following question. Please refer to the "Related question" for background

"In reality VIN pin has some current level during soft-start. I need to know this value.

If you can not correct the model then at least discribe the nature of this value for instance for 14V Vin supply.

Regards,
Andrey"

  • Hi Nikhil,
    The major current consumption is in the gate drive, which is supplied by VCC, and which is supplied by VIN through the internal LDO. The gate drive current is Cg x Vcc x Fsw, where Cg is the MOSFET total gate charge. Add about 3.5 to 4mA internal use, then you will get the VIN current during startup.

    Thanks,
    Youhao
  • Hi Youhao,
    is there some current limit for VIN pin.
    For example if Cvcc=10uF, then which maximum current will be for VIN to charge the Cvcc?

    thanks,
    Andrey
  • There is no VIN input current limit. The Input current is determined by its load: VCC load plus up to 4mA used by other internal circuit, but the VIN pin current may appear to be limited owing to the VCC current limit. Cvcc=10uF sounds big, taking longer time to charge up. We usually recommend 1uF. Please refer to the datasheet Applications Information section.