This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/TPS22945: minimum current limit accuracy

Part Number: TPS22945
Other Parts Discussed in Thread: TINA-TI, , TPS22941

Tool/software: TINA-TI or Spice Models

Hi, 

I have downloaded the transient spice model for the TPS22945 load switch and I  am testing it. I have modified it a bit to test the current limit accuracy and I see that when I load the output of the switch with a resistive load with values 70 ohms and lower (5V input and 5V on the ON pin) the switch enters an overcurrent condition and cycles according to the specifications in the datasheet. The issue is that the datasheet states clearly that the minimum current limit is at 100ma, which is not the case in the simulation. My understanding is that current limiting will not happen before 100ma. Shouldn't current limiting begin with values of 50 Ohms and lower and not also with higher ones i.e. 60 and 70 Ohms? The behavior that I am seeing matches that of figure 11 on the datasheet, but that contradicts the 100ma minimum current limit. Am I missing something? 

 Thanks in advance