This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100-Q1: TPS1H100-Q1 schematics

Part Number: TPS1H100-Q1

Hi Sir,.04_Sensor_Power.pdf

customer ask the TPS1H100-Q1 schematice confirm for bellows conditions

normal operation current ~0.25A
Current limit =0.3A

  • Hello,
    Schematic looks OK. here is my comment:
    1- Diode D401 forward voltage should be less than 0.6V in any circumstances
    2- The current limit set should be more than 500mA for meeting the 20% accuracy. 300mA current limit accuracy is not in the device specification

    Regards