This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65251: TPS65251 ENx pin behavior such as square wave

Part Number: TPS65251


Hello  all,

 When VIN is supplied from 4.4V to 4.8V, EN1 and EN2 pin have square wave such as attachied photo.

I couldn't find functional descrpition in the TPS65251 specification. Could you tell me why it is occured?

What trriger/specification does it happen? When PMIC detects it, What do ENx do?

Best Regards.,

Mitsuharu Iwasaki