Hi,
I've currently programmed a single ended BQ76PL455A-Q1 and am now looking to stack the devices, I have enabled all devices to trigger a Fault_N output if the Cell UV/OV and AUX UV faults are triggered. If these faults are triggered on a board higher up the stack will these faults automatically pass down the devices or do I have to enable the COMM_FAULT bit. Also if these are automatically passed down to the base device in the stack, is it possible to read which device triggered the initial fault?
Thanks,
Alex