This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

does this exist?



It would be nice to get a power bank with built-in wall plug (110~240V), built-in USB type C cable +/- C-to-lightning and C-to-microUSB adapters and a USB QC3.0 output port! Is anything like that available now or in the works? 

Availability of these features in power banks volume options, eg a slimmer (7-10mm thick) 5000MAh and a 10-13mm thick 10000MAh varieties that would be even more desirable. 
Future developments?
I would be grateful for your comments, info.
Marina 
  • Hi Marina,

    Welcome to e2e! Unformation we do not support QC3.0. Quick Charge 3.0 is NOT USB-PD compliant. We support voltages and currents per USB-PD specs: 5V/3A, 9V/3A, 15V/3A, 20V/5A. Also, currently we do not have any plans of supporting QC, only USB-PD.