We have a customer need an nanosecond conversion rate LDO.Is DC 5V input convert to DC 1.8V output, need the nanosecond conversion rate.
Can we have the Right Product?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have a customer need an nanosecond conversion rate LDO.Is DC 5V input convert to DC 1.8V output, need the nanosecond conversion rate.
Can we have the Right Product?
Thank you.
Hi Eric,
Customer the requirements for the LDO as below:
Iout max:500mA;
Package size:no requirement
Vin max:6.5
Vout tolerance:±3%
PSRR:80dB
Tks.
Hi Wilson:
Thank for your respond.Customer have found the right pruduct to their designe.