Hi,
I need to make a priority switch between 12V POE module (PD) and a 12V auxiliary power supply.
The POE has the highest priority (No EN signal).
I wonder if I can use the following architecture taken from the TPS25942A datasheet.
Considering:
1. The POE module need a minimal load to be present at start-up. What will happen if the auxiliary power is connected and then adding the POE.
2. The POE (PD) need to present a load in definite time, will the start up condition of the TPS25942 can meet the POE standard.
Thanks
Noam