How to calculate the maximum switching frequency that a gate driver can support? Is it related to the power dissipation that the device can withstand?
Let's say using UCC27524 as the gate driver in a boost controller, input voltage: 12V, output 30V/2A, how to estimate the maximum switching frequency with the UCC27524 in this case according to datasheet?
Thanks!