This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual output +50V and -50V DC/DC boost



Hi all,

i'm looking for DC/DC boost with dual output - one for +50V and the other for -50V.

The input voltage is between: 10V to 30V

and the load current from each output is ~5mA (so 10mA from each output should be suffice) . 

I don't want to use transformer in the design. 

Thanks a lot