This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25145: SW waveform issue

Part Number: LM25145

Dear Sir

Could you please help to check the attached for the SCH and layout for below spec design. Any advise please let me know.

Vin: 10.5V to 30V

Vout : 5V/12A

RRT:39KOhm

L:3.5uH

This is for BYD automotive power application and the EAU is over 200ku/y. Please kindly help to check the schematic and layout, customer will make the PCB if there are no problem for this design. very appreciate!

UEL070-M050E00-OP.SCH0456.UEL070-SCH0426.pdf1033.UEL070-M050E00-OP PCB(1).pdf