This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54040: TPS54040 input current at light load

Part Number: TPS54040


Dear Support team

I checked the input current by swinging the load of the TPS54040 from 10 mA to 100 mA.

Although the input current decreases linearly as Vin is increased, it seems that it increases only when Iout =10 mA. And value seems unstable at Iout=10mA

What is the reason for this?

It seems that the pulse skip mode is related, but is the current unstable at that time?

■Condition

Vin :11~16V Vout:1.5V Iout:10mA~100mA Fsw:400kHz

Regards

Tomohiro Nagasawa