This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33620: 12V to 3.8V application

Part Number: LMR33620
Other Parts Discussed in Thread: TPS22916

Hi Sir,

My customer would like to know if they apply a 4.2V on the output of LMR33620, will there any risk?

Below is the detail.

My customer are using LMR33620 on their platform for 12V to 3.8V application for their system and 12V is the main input source.

And on their system there is a li-battery will be charged by a boost circuit from the 3.8V.

When 12V is removed, the Li-battery will be switch to the output of LMR33620 to as a power source of the system.

Therefore, there will be a short time that 12V still on LMR33620 input while the Li-battery already supply to LMR33620 output.

Thanks,

Patrick