Other Parts Discussed in Thread: BQ34Z100-G1, BQSTUDIO
I am having an issue with BQ Studio connecting a bq34z100-G1 in HDQ module using the EV2400
When I use the older EV2300, BQ Studio automatically identifies the bq34z100-G1 and establishes communications without any issues
When the exact same setup is plugged into the EV2400, BQ Studio cannot auto detect the bq34z100-G1. Selecting the bq34z100-G1 manually also does not work, no data can be read
The EV2400 manual still claims that HDQ is not supported, but TI has confirmed on the forums that HDQ is supported in the latest firmware and the manual needs to be updated
This has been tested on multiple computers, the EV2300 with the add-on 64bit drivers works every time, but the EV2400 never is able to auto-detect or manually connect to the bq34z100-G1
Although I have a working setup using the EV2300, I would like to transition to the EV2400 if possible - Is there anything else that needs to be configured to get the EV2400 to work with this setup?