Tool/software: WEBENCH® Design Tools
I am using WEBENCH to size components for 12V to 5V Buck application using the LM5017. I have used LM5017 before, for 50V to 12V step down application(using Webench), and an inductor was recommended. But now everytime I try Webench, it is recommending a transformer with 2 outputs, whereas, I just need single output. Is there a setting within Webench that will let me decide that I just need to use an inductor only?