In the schematic of 300W PF circuit, schematic shows only two Switching mosfet used in boost converter. But in 1.2KW schematics PR779 shows 4 mosfet (Q3, Q4, Q5, Q6) for boosting. My doubt is why these two additional mosfets are used here? are they to increase the power rating of PFC circuit? If yes then while using UCC28070 IC how to calculate no of mosfets required to achieve the power rating?
Also what is the switching frequency used for 1.2KW PFC?