Other Parts Discussed in Thread: PMP15027
Hello
We are planning to use LM3410X as a flash driver in our design. For this we are following the circuit provided in datasheet in section 8.2.10 which shows 1.5A flash for 7.5V LED.
Our design needs only 1.1A for 7V LED (two 3.5V LEDs in series) getting power from a 1S battery.
What is the max duration of flash pulse that we can get?
Thanks
Kirti