Hi team
Could you let me know about if it is OK or not under the condition below?
1. It works correctly when it is decided the current by using ILIM and ICO.
2. CE_=LO without battery.
Best Regards,
Takanori Yuzawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team
Could you let me know about if it is OK or not under the condition below?
1. It works correctly when it is decided the current by using ILIM and ICO.
2. CE_=LO without battery.
Best Regards,
Takanori Yuzawa
Takanori-san,
Regarding 1, D+/D- detection determines whether the port is SDP, CDP, or DCP and sets the input current limit accordingly. The ILIM resistor clamps the maximum input current to a value which may be lower than the value set in the IINDPM register by D+/D- detection. If too much input current is pulled and the adapter starts to collapse, resulting in VINDPM activating, the ICO circuitry finds a new, lower input current limit value that prevents VINDPM.
Regarding 2, it is okay for /CE=LO without battery. This results in the battery pin voltage varying between recharge voltage and BATREG voltage as the charger varies between charging and not charging. The STAT pin blinks to indicate this.
Yes. ILIM allows you to clamp the input current limit. If the ILIM clamp isn't low enough then ICO actually finds the maximum power capability of the USB port.