Part Number: TPS55340
I've TPS55340s on multiple boards that suddenly don't work.
I used the Webench design tool, purchased the dev board and everything worked. I had 15 boards built using the design. The first one tested perfect.
The next 4 boards have all failed. When they are powered on, they start to audibly ring. They may or may not stop ringing. They don't output the boost voltage.
One of them, I turned it on, the meter read the output at 15VDC briefly, but then it stopped and went to the input voltage.
The first board tested is still silent and works great. About all I can figure, is I suddenly have a bunch of dead chips.
Input voltage is 12VDC @ 100kHz
Output voltage should be 15VDC
The enable is tied to the 12VDC rail and the soldering job the fab house did looks great. I've gone as far as, just to verify, as to reflow one of the boards. Still doesn't work.
ESD precautions have been used when handling the boards.
At present, best guess is I got a bad batch of TPS55340? I don't have any spares to replace for testing. I do still have other boards to test, but was hoping for something optimistic first.