This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60: 'Maximal Temperature = 0' vs 'Average Temperature = 1' in Settings:DA Configuration[CTEMP]?

Part Number: BQ40Z60


Hi,

Can you please explain/elaborate the difference between setting 'Maximal Temperature = 0' vs  'Average Temperature = 1' in Settings:DA Configuration[CTEMP]?

We have 4 thermistors and will use the internal temperature as a FET temperature so please verify these settings:

Settings:Temperature Enable, TS[4..1] = 1, Enabled

Settings: TSint = 1, Enabled

Settings: Temperature Mode, TSMode[4..1] = 0, cell

Settings: Temperature Mode, TSintMode = 1, FET

Settings: DA Configuration, CTEMP = ??

'Maximal Temperature = 0' vs  'Average Temperature = 1'

?Maximal Temperature = 0, Does Temperature() command return the highest of the 4 thermistors?? 

?Average Temperature = 1, Does Temperature() command return the average of the 4 thermistors??

Are my assumptions correct?

thanks,

Tom