This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28710: UL certification

Part Number: UCC28710


Hello Team,

One of my customer is looking for UL certification data for this device?

Is there any plan?

Regards,

Mahendra

  • Can you please make your request more specific? For example, UL certification in relation to what UL standards/regulation/policies?
  • I will close this string as the same question is answered and can be found by UCC28710 tag search. The below is a citation from the reply to the same question.

    "the UL status of the UCC28710: This particular part does not have UL certification or UL listing or UL file number. However, the mold-compound material used for its package is flame-rated to UL 94V-0.

    "TI does sometimes obtain UL Certification for a specific device or family of devices (such as in isolators or safety-related applications) based on market-driven requirements. Currently, there is no market requirement for UL certification for the UCC28710 or similar devices in this family. Regardless, all of TI packaging mold-compound material is flame-rated to UL94V-0 by internal policy."