This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for a DC-DC converter with external PWM signal (not for sync)

Other Parts Discussed in Thread: LM5114, LM3478

Hi,

I'm looking for a DC-DC converter/controller which can receive an external PWM instead of the internal one, not for synchronisation purpose.

The wanted topology is boost, buck-boost or flyback.

The input voltage is 3-5V and the output current is under 500mA.

I'd like to have an option in which the PWM signal is external, and when it's off, the output voltage is zero.

Please advise.

Thanks