This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54202: FIT / MTBF information in case of high junction temperature in continous operation mode

Part Number: TPS54202


Hi

The application converts an Input voltage of 24V to an Output voltage of 3.3V. The voltage Regulator is getting quite hot.

Are there any Information depending of junction temperature about the FIT / MTBF behaviour of this part?

Kind regards

Martin

  • You can estimate the junction temperature by using a thermal camera and the

    value of psiJT and the estimated power loss.

    If this value is less than 125C then the application should be OK.

    I do not think we can give any numbers for long term reliability.