I have a few questions about using an LED driver (15V 700mA CC driver) to power 3 LEDs with different Vf and forward current requirements:
Vf 3.2 - 3.6V 700mA
Vf 3.5 - 4.5V 750mA
Vf 3.4 - 4.0V 750mA
1. How does a CC led driver 'determine' the voltage that is needed in order to reach the 700mA?
2. What voltage will the driver provide at 700mA, is this 3x 3.5V = 10.5V? (because if 10.4V is provided, the Vf 3.5 of one of the LEDs is not met, so a current can't run: does it work this way?)
3. Will each LED draw 7.35W (10.5V x 700mA) /3 = 2.45W?
Thanks!