This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM317A: Linear regulator supplied backwards

Part Number: LM317A

Hello together,

we use the LM317A to make an output voltage of 5V from 12V.
During the production test, the output of the LM317A will be supplied with 9 V and the regulator input is open (floating).

Is this a problem for the LM317A? Will the regultator maybe even be destroyed or pre-damaged?

Thanks and best regards

Alex