This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV760: Thermal limit

Part Number: TLV760


Hi,

We are considering the TLV76012 for a design. We want the device to be short-circuit proof. The TLV760 is considered because it has a built-in temperature limit of 150°C. When testing its short-circuit behavior with a 13V input voltage, we noticed temperatures around 170°C on the outside of the package. 

To get a better feeling for the robustness of the device, we made an array of 30 short-circuited TLV760s. On this board, many devices failed upon power on. Of the remaining devices (about 10 of 30), several had temperatures in excess of 200°C on the outside.

What is the range of temperatures that can be expected for this device when short-circuited and how robust are the protections?

Thanks and regards,

Toby

  • Hi Toby,

    how many times have you barbecued the TLV760 before they failed?

    Kai
  • Hi Toby,

    The typical thermal shutdown temperature is 150ºC, but this is not a tight tolerance parameter and often will vary as much as 10 or 20ºC.

    For the parts that failed, did they no longer work or did they just fail to start up? Some LDOs with foldback current limit cannot start into a short. The output will not start up if OUT is shorted to GND.
  • Hi Toby,

    Another thing to note is dropout voltage, which is specified as max 1.2 V at Iout = 100 mA over temperature. Your devices may be operating in dropout with Vin = 13 V, Vout = 12 V.

    Using the thermal limit to provide short circuit protection is not recommended. Repeatedly entering thermal shutdown may degrade the reliability of the part as noted in the Absolute Maximum Ratings table of the datasheet.
  • Hi Kai,

    We had two boards, each with 30 devices. About 20 on each board died on startup.

    Toby

  • Hi Eric,
    We understand that there is significant spread on the temperature protection circuit. However, the datasheet reads on page one: "The device has robust internal thermal protection, which protects itself from potential damage caused by conditions like short to ground, increases in ambient temperature, high load, or high dropout events."

    We do not expect lifetime specifications to be met when the output is short circuited, but we do expect the device to survive a reasonable amount of time. I have tested several devices seperately and that worked well, although indeed there was significant spread on the steady-state temperatures. To get more confidence in its robustness we wanted to test many devices simultaneously and we made a test board. This lead to the failure of 2/3 of the devices. One device even had a hole in the package afterwards due to thermal stress. We had expected each device to scale back its short-circuit current such that it would operate at its temperature limit.

    So our question is: assuming that the output can be short-circuited in case of a fault, how can we use it in a way that it does not immediately break down?

    Thanks and regards,
    Toby
  • Hi Toby,

    Some linear regulators have a thermal or power limit that limits the power dissipation in the die, but does not shut the regulator down.

    Most devices have thermal shutdown protection where the regulator shuts down, the die cools, and the regulator turns back on at a lower temperature.

    I need to investigate which protection is designed into this regulator.

    How much distance do you have between the devices on your test board? You have to consider the heat from the other devices in addition to the heat generated within each linear regulator. It is possible the response time of the thermal protection is too slow and damage occurs to the die before thermal protection is activated.
  • Hi Toby,

    in section 10.1 datasheet says:

    "Use a ground reference plane, either embedded in the PCB itself or located on the bottom side of the PCB
    opposite the components. ... it behaves similarly to a thermal plane to spread heat from the linear regulator. In most applications, this ground plane is necessary to meet thermal requirements."

    So, the regulator needs the ground plane as part of the cooling. This is not surprising at all as the regulator comes in a tiny SOT23 package. And the temperature of this ground plane must be at a much lower temperature as the regulator itself. Otherwise it cannot dissipate the heat. Right? But if you mount directly next to the regulator another regulator which you barbecue in the same way and do this with 28 other regulators on the same PCB which you all barbecue at the same time, how shall the regulators be able to dissipate their heat? Do you really think that this absurd testing with 30 short-circuited SOT23 regulators all sitiing on the same PCB does make any reasonable sense?

    Kai
  • Hi Eric,

    What we have seen when testing a single component is that the regulator limits the current to keep the dissipation and die temperature constant at some value above 150°C. Looking at the block diagram in section 7.2 of the datasheet, we had expected this to be true irrespective of the ambient temperature. We thought the current would always be reduced to a level at which the die temperature is constant at the protection level. So indeed our test board has closely spaced TLV760s and heat from adjacent devices will have a significant impact on the temperature of a device.

    I have done some additional tests on a single device and found that the current is regulated to a minimum of about 45-50mA at high dissipation. This is also shown in figure 16 of the datasheet. When the dissipation is increased further by increasing the input voltage, the current drops slower than the voltage is increased. So the die gets hotter and hotter until it finally breaks down for temperatures above 200°C.

    Because in our appication, we need to consider relatively long periods for the output to be shorted, I think we need a stronger temperature feedback that regulates the current to whatever value required to keep the junction temperature constant.

    Thanks for your help, it is much appreciated.

    Best regards,

    Toby

  • Hi Kai,
    I guess I did not make sense to test the device in this manner, as it broke down. But from the description and block diagram, we had expected it to behave in a different manner, see also my reply to Eric's feedback. We'll be looking for a device that better suits our particular application. Thanks for your help.

    Regards,
    Toby
  • Hi Toby,

    you should not expect too much from this ultra tiny SOT23 package. The ground plane to which the regulator must be connected to, is part of the cooling management. Do you have such a ground plane in your application? The connection to ground plane changes the thermal flow within the chip. This has also influence on the thermal shutdown, because at these huge heats you get considerable temperature gradients, even within the chip. This can also be seen with many other chips: If the recommended cooling (heat sink, ground plane,...) is omitted the chip can overheat or the thermal shutdown can start delayed in spite of having a working thermal shutdown. So, it's extremely important to use the recommended cooling management, which is the mounting on a ground plane here.

    It's also important, that the temperature in the direct neighbourhood of regulator is normal, as normal as in a standard application. So, there should not sit other chips with a chip temperature of 170°C. It's very unusual to have this in a standard application. But if you have to expect this, you must improve your cooling management.

    You wrote:

    "When testing its short-circuit behavior with a 13V input voltage, we noticed temperatures around 170°C on the outside of the package. ... I have tested several devices seperately and that worked well, although indeed there was significant spread on the steady-state temperatures.."

    So, it worked as promised and expected! The failures occured only when you carried out your "flamethrower" test. :-) Right?

    Kai

  • Hi Kai,

    I had missed your message, hence my late reply.

    The problem we have with this IC is that it is not short-circuit proof under all conditions. If you short circuit the device while having a medium supply voltage the thermal protection works and the device becomes at bit warmer than 150°C. However, if the supply voltage is increased, the device becomes hotter and hotter, because the current is not scaled back as fast as the voltage is ramped up. This is also shown in figure 16 of the datasheet. If the voltage is ramped up futher, the device will fail before reaching the specified maximum supply voltage of 30V. This test was done at room temperature. We have products that have an ambient temperature of 80°C, so there isn't much thermal room to play with.

    The regulator is used to supply an interface to other products. In case there is a short-cicuit fault in the system, we don't want our product (of many hundreds of dollars) to be returned because a $0,13 LDO failed. We want the interface to be robust. 

    Regards,

    Toby

  • Hi Toby,

    yes, I understand what you mean. If your products have to run even at 80°C ambient temperature I would take a regulator in a bigger package.

    Kai