Other Parts Discussed in Thread: BQ24610, BQ24773, BQ24170, BQ25703A
Hello all,
I am new to battery technology and I am building an application with such requirement.
We will be using 3S 18650 Li-ion batteries to power a motor. So it then will be charged/monitored when the motor is not running, when the motor is running, the battery will not be charged. Which ICs should I be looking into to achieve such requirement? How can I prolong the life of battery in such application?
There are two options of power supply (12V/5A or 15V/4A) that I can choose to power the motor control MCU and also act as the charger adapter, which one should I choose? I assume the 15V/4A is better because the 3S charging voltage has to be greater than 12.6V since voltage of each cell is 4.2V at full charge, is that correct?.
Thanks,
Alex