Good day,
We are working on incorporating the TP2384 PoE PSE into our existing switch design so we followed there reference design in the TPS2384 Evaluation module (SLVU126D). The differences between this design and ours are as folows
1) I2C communication is not used so the clock, data and address pins are left floating
2) the device is always in auto mode (MS=0)
3) Only using 1 Port the rest are terminated according to (SLVA231A)
The issue is that the TPS2384 is able able to detect, classify and power an IEEE802.3af PD only once and afterwards the N pin is always grounded (Port 1). Measuring between RTN and this particular N pin if using a multi-meter in diode test shows a 0.7V drop.
Please correct me if I am wrong, If an Ethernet cable is not connected to the TPS2384 port the open circuit voltage is approximately 22V and when a cable is plugged in the detection cycle starts (4.4V and 8.8V) and in my case the voltage goes to approximately 48V with respect to RTN because the backup timer is implemented (ALTA/B == HIGH == 3.3V). This was observed the first time as expected.
But after a full detection, classify and power cycle, disconnecting the PD or even restarting the TPS2384 this particular pin is always 0V with respect to RTN which means that power is always supplied to the PD without classification or detection.
Whats causes this problem ? Is it possible that the TPS2384 chip is blown and if so why ?
Thank you,
Kind Regards,
Alexander M Ncube