Hi,
The corresponding battery model can be selected in Chemistry. However, due to the consideration of life problem, the voltage range is reduced from 2V-4.25V to 3-4V. And then the RSOC is not correct, but after learning, the result become more accurate. Considering long -distance transportation, select ship function(small self-consumption). While ship mode means shutdown, when restart RSOC will reduce from 100% to 75%.
Question: which mode should be selected?
Best regards,
Lenna