Hi,
I am designing an application which is powered through either of 2 sources rated 12V@6A. One is POE and other is through power Jack. I want to implement reverse current protection circuit implemented on my design so that POE output can be isolated in case DC Jack is used as power source. By default POE is used as power source but we may require to power the system through external DC source. Hence I want to have design like if DC Jack is used for power, it should not affect POE circuit. Also when POE is used as power source and in meantime DC source is plugged in, both should not get affected with each other.
Normally, we can think of using schottky diode on output of both POE and DC source but since the power requirement is more(60-70W), we don't want to waste power(which comes to be 4-5W) specially POE power.
Can anyone please suggest solution for this design?
Regards
Narendra Singh