Part Number: BQ78350-R2-DEVICE-FW
Hello,
We have just designed a new BMS for a 7S pack for a special power tool, using bq78350-R2.
We need to set some protections like OCD Threshold and SOCD Threshold around -40A and -50A, but these values exceed the max allowed programmable value of -32768mA.
I understand the role of the IPScale parameter, but it is unclear the usage:
If I set IPSCALE = 0x01 (bit15-12= 0001), I understand that some readings are scaled by a factor of 10^1, but I don't understand which settings need to be saved in the DataFlash scaled by 10, and which not:
- do ALL the current settings expressed in mA need to be scaled ?
- do ALL the capacity settings expressed in mAh need to be scaled ?
If only a part of the parameters need to be scaled, which one are affected by the IPSCALE ? and which not ?
Thanks in advance.
Pietro