Hello,
I was hoping to get this attached schematic reviewed. I wish to only use the AC input, so I am not sure if I should leave the USBPG floating as is? Also, I would like to use 2000mAh or less LiPo batteries, so is it okay to have the charge current at ISET1 be at 1A? Will it be detrimental to the battery life? Is it advisable to increase the resistance at ISET1 to 2k to get the max charge current to around 500mA? If I make this change will I have to modify the safety timer resistor value too?. Thanks!