This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Robert,
Is the part turned on with the output voltage high before it is turned off? The TPS22910A does not have any sort of output discharge integrated, so if you don't have a resistor on the output then it will be left floating instead of being pulled down. What is on the output of the device?
Thanks,
Alek Kaknevicius
Hi Alek,
Thanks for your response.
1. The part is turned on, with the output voltage high, before attempting to disable it.
2. Although there is no single resistor to ground on its output, the TPS22910A is connected to a BQ27246 gas gauge, and then to a TLV7113318DDSET to feed an entire circuit that takes about 8mA standing current. I can't see that sustaining a floating voltage for very long. In addition, if I was seeing a floating voltage, it would remain even if I disconnect the input to the TPS22910A, but as soon as I do that, the output collapses. Therefore, my conclusion is still that, despite the fact that I measured 5V on the enable pin, the TPS22910A has not turned off.
Any further comments would be most welcome and appreciated.
Regards,
Rob
H Rob,
Do you see the same voltage on the output as the input, or is it lower? This can help us determine whether the switch is completely ON, completely OFF, or not behaving as expected (partially ON).
Thanks,
Alek Kaknevicius