Part Number: LM5116
Hi,
I have designed a 20A DC DC Converter using LM5116 IC for an output of 14.5V. I performed short circuit test for my board (an input of around 70V was provided) . But the IC failed after short circuit protection test. Should i add any protection circuit at the output to protect it from damaging the unit (in the field, since my application is an automotive one).