Dear All:
It is now verified that the Hybrid power boost mode will have an action.
Find a relationship with watchdog timeout.
For example, our EC will set ChargeCurrent() to zero when it is full.
This results in a watchdog timeout.
The Hybrid power boost mode is turned off (the above is my conjecture, because it is not certain that the TIME OUT is triggered, there is no place to see if it is triggered)
So just a couple of question as below:.
1. what is the main function of ChargeCurrent() &ChargeVoltage() ? Is it to be set only one time or consider the actual situation, such as filling up, or the protection of dynamic modulation ChargeVoltage(),ChargeCurrent()
2 . What else does this TIMEOUT want to protect?
To understand the purpose, the set value will meet the purpose of this function.