Other Parts Discussed in Thread: BQSTUDIO
We have designed a custom implementation of the BQ40Z60, closely based off of the EVM design. The major changes were: using pairs of parallel FETs (BSC090INS) instead of the single charge and discharge FETs, to allow for higher peak discharge currents. We also changed the output inductor and capacitors to allow for a charge rate of 4.5A. Our battery is a 4S4P LiIon pack, with a total capacity of 200Wh.
We have encountered a rather puzzling issue when attempting to discharge the packs at a relatively high (28A) current.
Here are the symptoms and diagnostic steps so far:
1: With all protections disabled (Enabled Protections A through D all set to 0), attaching a load that draws 28A causes the CHG and DSG FETs to stay on for only 30ms before shutting off for one second before turning on for another 30ms. The BMS keeps switching the FETs on and off this way, with 30ms pulses at exactly 1 Hz. In BQStudio and in the logs, the CHG and DSG enable bits on Operation Status A can be observed to turn off. But none of the protection or safety status bits are activated during this. The other strange thing that happens is the discharge currents in the cells are very imbalanced when this is happening, one cell appears to have very high current as indicated in BQstudio, while the other cells have almost no current. See “discharge_test_RSNS0.log”
2: After some trial and error, we found that we can get the cycling of the FETs to stop, and for the pack to discharge normally with the 28A load, by simply changing the RSNS bit from 0 to 1. (See “discharge_test_RSNS1.log”) According to the TRM, the RSNS bit doubles the sense resistor voltage thresholds that trigger the AOLD, ASCC, ASCD1 and ASCD2 overload and short circuit protections. I can understand how a high current could trigger van overload, and how doubling the voltage threshold could cause the triggering to stop. But I don’t understand why a protection that is disabled, and that has not been recorded or indicated as having triggered, would be activating at all. Shouldn’t disabling all protections mean that discharge should not be limited by the BMS at all? We do not actually plan to disable all the protections in practice, but we simply want to verify that we have control over them, and that none ever trigger in an undesired and unexpected manner.
What do you think is causing this behavior?
Mon May 21 16:26:15 EDT 2018 Device Name = bq40z60 Firmware Version = V0_15_BLD0021 Design Capacity = 2112 Design Voltage = 14400 Specification Info = 0x0031 Manufacturer Date = 1980-1-1 Serial Number = 0x0001 Manufacturer Name = Texas Instruments Device Name = bq40z60 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,RunTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,TurboPwr,TurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,ChgrStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,Vacp,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,CBTime1,CBTime2,CBTime3,CBTime4,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,ChgVoltReg,ChgCurrReg,LogRowTime(ms),LogStatus 1,2018-05-21 16:26:19,4.178,0x01C7,4320,10,0xE081,0,65535,65535,1,27.8,16573,-14,-14,100,0,0,0,57098,47663,47663,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4144,4143,4144,4143,16574,0,-21,-19,-26,-38,-9,-8,-11,-16,-22,-24,25.8,27.6,27.8,27.5,27.0,27.8,-273.2,13011,18271,13439,18817,13011,18271,3,5,13439,18817,31.4,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,727,3,3,3,3,425,541,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,425,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1075,SUCCESS 2,2018-05-21 16:26:23,8.170,0x01C7,4320,10,0xE081,0,65535,65535,1,27.8,16573,-15,-14,100,0,0,0,57098,43850,47663,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4144,4143,4144,4143,16571,0,-19,-22,-22,-34,-8,-9,-9,-14,-25,-24,25.9,27.6,27.8,27.5,27.0,27.8,-273.2,13011,18271,13439,18817,13011,18271,3,5,13439,18817,31.4,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,731,3,3,3,3,425,541,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,425,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1077,SUCCESS 3,2018-05-21 16:26:27,12.163,0x01C7,4320,10,0xE081,0,65535,65535,1,27.8,16574,-14,-14,100,0,0,0,57098,47663,47663,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4144,4143,4144,4143,16570,0,-25,-23,-25,-27,-10,-10,-10,-11,-25,-24,25.9,27.6,27.8,27.5,27.0,27.8,-273.2,13011,18271,13439,18817,13011,18271,3,5,13439,18817,31.4,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,735,3,3,3,3,425,541,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,425,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1061,SUCCESS 4,2018-05-21 16:26:31,16.174,0x01C7,4320,10,0xE081,0,65535,65535,1,27.8,16574,-15,-15,100,0,0,0,57098,43850,43850,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C1,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4144,4143,4144,4141,16561,6,-5,-7,-2,-269,-2,-3,-1,-111,-1468,-1477,25.9,27.6,27.8,27.5,27.0,27.8,-273.2,13011,18271,13439,18817,13011,18271,3,5,13439,18817,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,0,3,3,3,3,425,541,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,425,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1060,SUCCESS 5,2018-05-21 16:26:35,20.162,0x01C1,4320,10,0xE081,0,65535,65535,1,27.8,16566,-880,-890,100,0,0,0,57098,752,744,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C1,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4087,4137,4141,4140,16554,1,-5402,-6,-3,-7,-2208,-2,-1,-3,-1456,-1473,25.9,27.6,27.8,27.4,27.0,27.8,-273.2,13010,18270,13439,18817,13008,18285,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,4,3,3,3,3,426,542,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,426,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1050,SUCCESS 6,2018-05-21 16:26:39,24.177,0x01C1,4320,10,0xE081,0,65535,65535,1,27.8,16563,-876,-888,100,0,0,0,57098,755,745,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C1,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4086,4136,4140,4140,16552,1,-5399,-4,-4,-3,-2206,-2,-2,-1,-1451,-1469,25.9,27.6,27.8,27.5,27.0,27.8,-273.2,13010,18269,13439,18817,13007,18283,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,8,3,3,3,3,427,544,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,427,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1059,SUCCESS 7,2018-05-21 16:26:43,28.172,0x01C1,4320,10,0xE081,0,65535,65535,1,27.8,16560,-880,-886,100,0,0,0,57098,752,747,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C1,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4086,4136,4140,4139,16550,1,-5400,-4,-1,-5,-2206,-2,0,-2,-1452,-1467,26.0,27.6,27.8,27.4,27.0,27.8,-273.2,13010,18268,13439,18817,13006,18281,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,12,3,3,3,3,428,546,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,428,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1027,SUCCESS 8,2018-05-21 16:26:47,32.165,0x01C1,4320,10,0xE081,0,65535,65535,1,27.8,16558,-878,-885,100,0,0,0,57098,754,748,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C1,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4085,4135,4139,4139,16550,0,-5401,-3,2,-7,-2206,-1,1,-3,-1450,-1464,26.0,27.6,27.8,27.4,26.9,27.8,-273.2,13010,18267,13439,18817,13005,18280,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,16,3,3,3,3,429,547,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,429,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1059,SUCCESS 9,2018-05-21 16:26:51,36.173,0x01C1,4320,10,0xE081,0,65535,65535,1,27.8,16557,-877,-883,100,0,0,0,57098,755,750,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C1,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4085,4135,4139,4138,16546,1,-5399,-6,-3,-4,-2205,-2,-1,-2,-1452,-1462,26.0,27.6,27.8,27.4,27.0,27.8,-273.2,13010,18267,13439,18817,13004,18278,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,20,3,3,3,3,430,549,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,430,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1076,SUCCESS 10,2018-05-21 16:26:55,40.167,0x01C1,4320,10,0xE081,0,65535,65535,1,27.8,16555,-879,-882,100,0,0,0,57098,753,751,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C1,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4084,4134,4138,4138,16544,0,-5398,-4,-3,-4,-2205,-2,-1,-2,-1453,-1461,26.0,27.6,27.8,27.4,27.0,27.8,-273.2,13010,18267,13439,18817,13003,18276,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,24,3,3,3,3,431,551,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,431,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1075,SUCCESS 11,2018-05-21 16:26:59,44.176,0x01C1,4320,10,0xE081,0,65535,65535,1,27.8,16554,-880,-882,100,0,0,0,57098,752,751,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C1,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4084,4134,4138,4137,16544,0,-5399,-7,-2,-4,-2205,-3,-1,-2,-1451,-1459,26.0,27.6,27.8,27.4,26.9,27.8,-273.2,13010,18267,13439,18817,13002,18275,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,28,3,3,3,3,432,552,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,432,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1044,SUCCESS 12,2018-05-21 16:27:03,48.170,0x01C1,4320,10,0xE081,0,65535,65535,1,27.8,16559,-15,-770,100,0,0,0,57098,43838,860,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4140,4139,4140,4139,16556,1,-25,-23,-18,-34,-10,-10,-7,-14,-23,-1275,26.1,27.6,27.8,27.4,27.0,27.8,-273.2,13010,18266,13439,18817,13002,18275,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,32,3,3,3,3,432,552,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,432,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1075,SUCCESS 13,2018-05-21 16:27:07,52.171,0x01C7,4320,10,0xE081,0,65535,65535,1,27.8,16562,-14,-15,100,0,0,0,57098,47650,43838,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xD0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4141,4140,4141,4140,16557,0,-23,-22,-23,-39,-10,-9,-10,-16,-26,-25,26.1,27.6,27.8,27.4,27.0,27.8,-273.2,13010,18266,13439,18817,13002,18275,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,1,3,3,3,3,432,552,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,432,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1038,SUCCESS 14,2018-05-21 16:27:11,56.173,0x01C7,4320,10,0xE081,0,65535,65535,1,27.8,16563,-15,-15,100,0,0,0,57098,43838,43838,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xD0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4141,4140,4141,4140,16558,6,-25,-24,-20,-39,-10,-10,-8,-16,-23,-25,26.0,27.6,27.8,27.4,27.0,27.8,-273.2,13010,18266,13439,18817,13002,18275,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,5,3,3,3,3,432,552,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,432,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1075,SUCCESS 15,2018-05-21 16:27:15,60.164,0x01C7,4320,10,0xE081,0,65535,65535,1,27.8,16564,-13,-15,100,0,0,0,57098,49816,43838,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xD0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4142,4141,4142,4140,16557,0,-21,-24,-24,-28,-9,-10,-10,-12,-23,-25,26.0,27.6,27.8,27.4,27.0,27.8,-273.2,13010,18266,13439,18817,13002,18275,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,9,3,3,3,3,432,552,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,432,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1062,SUCCESS
Mon May 21 16:27:48 EDT 2018 Device Name = bq40z60 Firmware Version = V0_15_BLD0021 Design Capacity = 2112 Design Voltage = 14400 Specification Info = 0x0031 Manufacturer Date = 1980-1-1 Serial Number = 0x0001 Manufacturer Name = Texas Instruments Device Name = bq40z60 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,RunTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,TurboPwr,TurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,ChgrStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,Vacp,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,CBTime1,CBTime2,CBTime3,CBTime4,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,ChgVoltReg,ChgCurrReg,LogRowTime(ms),LogStatus 1,2018-05-21 16:27:53,4.001,0x01C7,4320,10,0xE081,0,65535,65535,1,27.7,16568,-14,-15,100,0,0,0,57098,43838,43838,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xD0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4143,4142,4143,4142,16565,1,-26,-25,-20,-30,-11,-10,-8,-12,-23,-24,25.9,27.6,27.7,27.4,26.9,27.7,-273.2,13010,18266,13439,18817,13002,18275,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,47,3,3,3,3,432,552,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,432,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1050,SUCCESS 2,2018-05-21 16:27:57,8.001,0x01C7,4320,10,0xE081,0,65535,65535,1,27.7,16569,-15,-14,100,0,0,0,57098,47650,47650,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xD0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4143,4142,4143,4142,16565,4,-23,-27,-22,-33,-10,-11,-9,-14,-23,-24,25.9,27.6,27.7,27.4,26.9,27.7,-273.2,13010,18266,13439,18817,13002,18275,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,51,3,3,3,3,432,552,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,432,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1075,SUCCESS 3,2018-05-21 16:28:01,12.001,0x01C7,4320,10,0xE081,0,65535,65535,1,27.7,16569,-15,-14,100,0,0,0,57098,43838,47650,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xD0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4143,4142,4143,4142,16564,1,-24,-21,-23,-20,-10,-9,-10,-8,-23,-24,25.9,27.5,27.7,27.4,26.9,27.7,-273.2,13010,18266,13439,18817,13002,18275,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,55,3,3,3,3,432,552,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,432,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1037,SUCCESS 4,2018-05-21 16:28:05,16.001,0x01C7,4320,10,0xE081,0,65535,65535,1,27.7,16569,-15,-14,100,0,0,0,57098,47650,47650,65535,4400,16520,0x00C0,0,-3022,-1917,99,0x01C7,0x0000,0x10,0x0008,0x0000,0xD0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4143,4142,4143,4142,16565,1,-21,-19,-28,-18,-9,-8,-12,-7,-23,-24,25.9,27.6,27.7,27.4,26.9,27.7,-273.2,13010,18266,13439,18817,13002,18275,3,5,13437,18832,27.8,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,59,3,3,3,3,432,552,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,432,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1046,SUCCESS 5,2018-05-21 16:28:09,20.002,0x01C7,4320,10,0xE081,0,65535,65535,1,26.1,15159,-29904,-7743,100,0,0,0,57098,33,93,65535,4400,16520,0x00C0,0,-11425,-17617,99,0x01C7,0x0000,0x10,0x0004,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3772,3789,3793,3794,15151,50,-29611,-29608,-29606,-29595,-11169,-11218,-11230,-11228,-32767,-12842,26.0,25.2,25.3,25.0,24.6,26.0,-273.2,12998,18247,13439,18817,12986,18248,3,5,13440,18834,27.5,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,2,3,3,3,3,453,584,4,0,0,0,0,13800,13800,13800,13800,3,3,3,3,453,4,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1070,SUCCESS 6,2018-05-21 16:28:13,24.002,0x01C7,4320,10,0xE081,0,65535,65535,1,26.7,15074,-29403,-12983,100,0,0,0,57098,33,56,65535,4400,16520,0x00C0,0,-16554,-27175,99,0x01C7,0x0000,0x10,0x0004,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3751,3768,3772,3773,15073,50,-29376,-29379,-29379,-29379,-11019,-11070,-11082,-11085,-32767,-17631,27.0,25.2,25.4,25.0,24.6,26.9,-273.2,12965,18198,13439,18817,12954,18200,3,5,13440,18834,27.5,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,6,3,3,3,3,483,629,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,485,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1079,SUCCESS 7,2018-05-21 16:28:17,28.002,0x01C7,4320,10,0xE081,0,65535,65535,1,27.7,15019,-29282,-16914,100,0,0,0,57098,33,43,65535,4400,16520,0x00C0,0,-20450,0,99,0x01C7,0x0000,0x10,0x0004,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3738,3755,3759,3761,15021,51,-29260,-29260,-29267,-29260,-10937,-10987,-11001,-11005,-32767,-21268,27.9,25.2,25.4,25.1,24.7,27.9,-273.2,12932,18149,13439,18817,12921,18150,3,5,13440,18834,27.5,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,10,3,3,3,3,516,679,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,518,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1073,SUCCESS 8,2018-05-21 16:28:21,32.002,0x01C7,4320,10,0xE081,0,65535,65535,1,28.7,14979,-29192,-19876,100,0,0,0,57098,33,36,65535,4400,16520,0x00C0,0,-23410,0,99,0x01C7,0x0000,0x10,0x0004,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3728,3746,3749,3751,14984,51,-29184,-29176,-29186,-29179,-10880,-10929,-10942,-10945,-32767,-24032,28.9,25.3,25.5,25.2,24.8,28.9,-273.2,12900,18100,13439,18817,12889,18102,3,5,13440,18834,27.5,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,14,3,3,3,3,550,730,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,550,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1082,SUCCESS 9,2018-05-21 16:28:25,36.002,0x01C7,4320,10,0xE081,0,65535,65535,1,29.6,14950,-29123,-22107,100,0,0,0,57098,33,33,65535,4400,16520,0x00C0,0,-25659,0,99,0x01C7,0x0000,0x10,0x0004,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3721,3739,3742,3743,14954,54,-29114,-29113,-29122,-29112,-10833,-10885,-10897,-10897,-32767,-26131,29.7,25.4,25.5,25.3,24.8,29.7,-273.2,12867,18052,13439,18817,12856,18053,3,5,13440,18834,27.5,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,18,3,3,3,3,581,776,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,583,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1074,SUCCESS 10,2018-05-21 16:28:29,40.003,0x01C7,4320,10,0xE081,0,65535,65535,1,30.3,14926,-29067,-23787,100,0,0,0,57098,33,33,65535,4400,16520,0x00C0,0,-27367,0,99,0x01C7,0x0000,0x10,0x0004,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3715,3733,3736,3738,14933,53,-29056,-29060,-29064,-29059,-10794,-10848,-10858,-10862,-32767,-27726,30.4,25.5,25.7,25.4,25.0,30.4,-273.2,12835,18004,13439,18817,12824,18005,3,5,13440,18834,27.5,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,22,3,3,3,3,613,824,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,615,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1084,SUCCESS 11,2018-05-21 16:28:33,44.003,0x01C7,4320,10,0xE081,0,65535,65535,1,30.9,14907,-29022,-25051,100,0,0,0,57098,33,33,65535,4400,16520,0x00C0,0,-28665,0,99,0x41C7,0x0000,0x20,0x0314,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3714,3728,3732,3733,14914,54,-29040,-29023,-29013,-29020,-10785,-10820,-10828,-10833,-32767,-28937,31.2,25.7,25.8,25.5,25.1,31.2,-273.2,12803,17956,13439,18817,12792,17957,3,5,13440,18834,27.5,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,26,3,3,3,3,645,872,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,645,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1030,SUCCESS 12,2018-05-21 16:28:37,48.003,0x41C7,4320,10,0xE081,0,65535,65535,1,31.7,14892,-28985,-26001,100,0,0,0,57098,33,33,65535,0,0,0x00C0,0,-29651,0,99,0x41C7,0x0000,0x20,0x0014,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3707,3725,3728,3730,14900,53,-28975,-28980,-28983,-28985,-10741,-10795,-10805,-10811,-32767,-29858,31.8,25.8,26.0,25.6,25.2,31.8,-273.2,12771,17908,13439,18817,12759,17908,3,5,13440,18834,27.5,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,30,3,3,3,3,678,921,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,680,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1102,SUCCESS 13,2018-05-21 16:28:41,52.003,0x41C7,4320,10,0xE081,0,65535,65535,1,32.3,14880,-28953,-26714,100,0,0,0,57098,33,33,65535,0,0,0x00C0,0,-30400,0,99,0x41C7,0x0000,0x20,0x0014,0x0000,0xC0,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3704,3722,3726,3727,14888,55,-28937,-28950,-28944,-28950,-10718,-10775,-10785,-10790,-32767,-30557,32.3,26.0,26.0,25.9,25.3,32.3,-273.2,12738,17860,13439,18817,12727,17860,3,5,13440,18834,27.5,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,34,3,3,3,3,710,969,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,710,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1049,SUCCESS 14,2018-05-21 16:28:45,56.004,0x41C7,4320,10,0xE081,0,65535,65535,0,32.8,14869,-28922,-27249,100,0,0,0,9920,0,0,65535,0,0,0x0BD0,0,-30968,0,99,0x41C7,0x0000,0x20,0x0014,0x0000,0xC5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3701,3719,3723,3724,14879,53,-28914,-28926,-28919,-28921,-10701,-10758,-10767,-10770,-32767,-31088,32.9,26.1,26.2,25.9,25.5,32.9,-273.2,-20,-20,725,992,-20,-20,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,38,3,3,3,3,742,1007,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,744,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1105,SUCCESS 15,2018-05-21 16:28:49,60.004,0x41C7,4320,10,0xE081,0,65535,65535,0,33.3,14860,-28902,-27648,100,0,0,0,9920,0,0,65535,0,0,0x0BD0,0,-31401,0,99,0x41C7,0x0000,0x20,0x0014,0x0000,0xC5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3702,3718,3722,3722,14868,53,-28911,-28906,-28898,-28900,-10703,-10747,-10756,-10757,-32767,-31491,33.4,26.2,26.3,26.1,25.6,33.4,-273.2,-52,-52,725,992,-52,-52,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,42,3,3,3,3,774,1039,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,776,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1066,SUCCESS 16,2018-05-21 16:28:53,64.004,0x41C7,4320,10,0xE081,0,65535,65535,0,33.7,14852,-28876,-27946,100,0,0,0,9920,0,0,65535,0,0,0x0BD0,0,-31729,0,99,0x41C7,0x0000,0x20,0x0014,0x0000,0xC5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3697,3715,3719,3720,14861,53,-28866,-28875,-28874,-28871,-10672,-10727,-10738,-10740,-32767,-31798,33.9,26.4,26.5,26.3,25.8,33.9,-273.2,-84,-84,725,992,-84,-84,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,46,3,3,3,3,806,1071,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,808,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1076,SUCCESS 17,2018-05-21 16:28:57,68.004,0x41C7,4320,10,0xE081,0,65535,65535,0,34.2,14846,-28860,-28167,100,0,0,0,9920,0,0,65535,0,0,0x0BD0,0,-31979,0,99,0x41C7,0x0000,0x20,0x0014,0x0000,0xC5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3695,3713,3717,3718,14853,54,-28846,-28856,-28848,-28849,-10659,-10714,-10723,-10726,-32767,-32031,34.3,26.6,26.6,26.4,26.0,34.3,-273.2,-116,-116,725,992,-116,-116,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,50,3,3,3,3,838,1103,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,840,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1085,SUCCESS 18,2018-05-21 16:29:01,72.004,0x41C7,4320,10,0xE081,0,65535,65535,0,34.7,14838,-28834,-28330,100,0,0,0,9920,0,0,65535,0,0,0x0BD0,0,-32168,0,99,0x41C7,0x0000,0x20,0x0014,0x0000,0xC5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3693,3711,3716,3717,14849,54,-28827,-28835,-28835,-28831,-10646,-10701,-10715,-10716,-32767,-32208,34.8,26.7,26.8,26.6,26.1,34.8,-273.2,-148,-148,725,992,-148,-148,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,54,3,3,3,3,870,1135,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,872,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1095,SUCCESS 19,2018-05-21 16:29:05,76.005,0x41C7,4320,10,0xE081,0,65535,65535,0,35.1,14833,-28819,-28449,100,0,0,0,9920,0,0,65535,0,0,0x0BD0,0,-32312,0,99,0x41C7,0x0000,0x20,0x0014,0x0000,0xC5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3691,3710,3714,3715,14842,53,-28809,-28811,-28816,-28811,-10633,-10689,-10702,-10703,-32767,-32342,35.3,26.9,26.9,26.8,26.3,35.2,-273.2,-180,-180,725,992,-180,-180,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,58,3,3,3,3,902,1167,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,902,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1054,SUCCESS 20,2018-05-21 16:29:09,80.005,0x41C7,4320,10,0xE081,0,65535,65535,0,35.5,14827,-28804,-28536,100,0,0,0,9920,0,0,65535,0,0,0x0BD0,0,-32421,0,99,0x41C7,0x0000,0x20,0x0014,0x0000,0xC5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3690,3709,3713,3714,14837,53,-28804,-28795,-28801,-28794,-10629,-10680,-10694,-10694,-32767,-32444,35.6,27.0,27.1,26.9,26.4,35.6,-273.2,-212,-212,725,992,-212,-212,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,62,3,3,3,3,934,1199,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,934,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1049,SUCCESS 21,2018-05-21 16:29:13,84.005,0x41C7,4320,10,0xE081,0,65535,65535,0,36.0,15988,-14,-25242,100,0,0,0,9920,0,0,65535,0,0,0x0BD0,0,-32466,0,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xC5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4006,4002,4005,4000,16001,5,-23,-18,-27,-26,-9,-7,-11,-10,-22,-26927,36.0,29.7,29.8,29.7,29.1,36.0,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,66,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1058,SUCCESS 22,2018-05-21 16:29:17,88.005,0x41C3,4320,10,0xE081,0,65535,65535,0,35.9,16074,-15,-13,100,0,0,0,9920,0,0,65535,0,0,0x03D0,0,-3022,-1928,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xD5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4022,4021,4024,4019,16086,117,-19,-22,-27,-30,-8,-9,-11,-12,-23,-21,35.6,29.8,29.9,29.8,29.2,35.6,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,1,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1083,SUCCESS 23,2018-05-21 16:29:21,92.006,0x41C3,4320,10,0xE081,0,65535,65535,0,35.0,16124,-15,-13,100,0,0,0,9920,0,0,65535,0,0,0x03D0,0,-3022,-1931,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xD5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4033,4032,4034,4030,16128,227,-22,-23,-18,-31,-9,-9,-7,-12,-24,-22,34.9,30.0,30.1,29.9,29.4,34.9,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,5,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1060,SUCCESS 24,2018-05-21 16:29:25,96.006,0x41C3,4320,10,0xE081,0,65535,65535,0,34.7,16160,-14,-14,100,0,0,0,9920,0,0,65535,0,0,0x03D0,0,-3022,-1931,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xD5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4042,4041,4043,4040,16168,2,-27,-22,-23,-28,-11,-9,-9,-11,-23,-22,34.6,30.1,30.2,30.0,29.5,34.6,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,9,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1070,SUCCESS 25,2018-05-21 16:29:29,100.006,0x41C3,4320,10,0xE081,0,65535,65535,0,34.5,16189,-14,-14,100,0,0,0,9920,0,0,65535,0,0,0x03D0,0,-3022,-1931,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xD5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4053,4049,4050,4047,16199,0,-29,-26,-25,-30,-12,-11,-10,-12,-24,-22,34.5,30.2,30.2,30.1,29.5,34.5,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,13,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1063,SUCCESS 26,2018-05-21 16:29:33,104.006,0x41C3,4320,10,0xE081,0,65535,65535,0,34.5,16213,-14,-14,100,0,0,0,9920,0,0,65535,0,0,0x03D0,0,-3022,-1927,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xD5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4055,4054,4056,4053,16214,1,-20,-22,-24,-32,-8,-9,-8,-13,-23,-23,34.4,30.2,30.3,30.2,29.5,34.4,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,17,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1071,SUCCESS 27,2018-05-21 16:29:37,108.007,0x41C3,4320,10,0xE081,0,65535,65535,0,34.3,16232,-14,-14,100,0,0,0,9920,0,0,65535,0,0,0x03D0,0,-3022,-1927,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xD5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4059,4058,4060,4057,16233,2,-11,-21,-26,-31,-4,-9,-11,-13,-23,-23,34.2,30.2,30.3,30.2,29.6,34.2,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,21,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1049,SUCCESS 28,2018-05-21 16:29:41,112.007,0x41C3,4320,10,0xE081,0,65535,65535,0,34.1,16249,-15,-14,100,0,0,0,9920,0,0,65535,0,0,0x03D0,0,-3022,-1927,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xD5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4063,4062,4064,4061,16251,0,-14,-25,-22,-34,-6,-10,-9,-14,-24,-23,34.0,30.3,30.4,30.2,29.6,34.0,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,25,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1074,SUCCESS 29,2018-05-21 16:29:45,116.007,0x41C3,4320,10,0xE081,0,65535,65535,0,33.9,16263,-15,-14,100,0,0,0,9920,0,0,65535,0,0,0x03D0,0,-3022,-1927,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xD5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4066,4066,4067,4064,16263,5,-23,-23,-22,-37,-9,-9,-9,-15,-23,-23,33.8,30.3,30.5,30.2,29.6,33.8,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,29,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1068,SUCCESS 30,2018-05-21 16:29:49,120.007,0x41C3,4320,10,0xE081,0,65535,65535,0,33.7,16275,-14,-14,100,0,0,0,9920,0,0,65535,0,0,0x03D0,0,-3022,-1927,99,0x41C3,0x0000,0x20,0x0018,0x0000,0xD5,0x0918,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4070,4069,4071,4068,16276,0,-19,-20,-25,-32,-8,-8,-10,-13,-21,-23,33.8,30.3,30.5,30.2,29.6,33.8,-273.2,-220,-220,725,992,-220,-220,3,5,725,992,32.6,24.0,1000,1000,1000,1000,0,0,0,0,1,4,1,1,1,1,33,3,3,3,3,942,1207,5,0,0,0,0,13800,13800,13800,13800,3,3,3,3,942,5,1.0,1000,4,4,4,4,0,0,0,0,0,0,0,0,0,13533,19658,0,0,1077,SUCCESS