Other Parts Discussed in Thread: BQ24640
Dear Sir,
Vin: 18V~32.2V
Constant Average Current: up to 2.5A
Charge voltage of Super Capacitor: 28V
Use the chip to charge the super capacitor by constant current (2.5A maximum)
And can cut off the charge path when the voltage of super capacitor reaches 28V.
It should be charged again automatically when the voltage drops below 28V.
It's better to have super capacitor voltage monitored, and have a dedicated pin to indicate the super capacitor status.
Please help to recommend a part which can satisfy above requirements.
Thanks.