Hello,
We are developing an application where we intend to use a BQ25895 with a 1 cell Li-Ion battery as a power bank: we need to be able to charge the battery from VBUS, and output 5V@3.1A on PMID to charge external devices. we are using the BQ25895 in host mode with a microcontroller that talks to it over I2C. have some questions pls clarify.
From what I understand, if only VBUS is present, the internal converter will be in buck mode charging the battery,
1. When VBUS is present will get 5V@3.2A at PMID but will it simultaneously charge battery Icharge@5A ?
Regards,
Raghu