This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61021A: Pull-down resistor on enable pin

Part Number: TPS61021A


Hello,

Is there an internal pull-down resistor on the enable pin in the TPS61021A or is it recommanded to add an external one ? 

I didn't find this information in the datasheet.


Thank you

Guillaume

  • the EN pin is of high impedance, it doesn't has internal pull down resistor. you can add an external resistor. the value can be a range, around 10k is OK. this resistor can be helpful if the board layout is not good or in high ESD condition.