This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: GPOUT pin configuration

Part Number: BQ27510-G3

If I set the Op Config [PFC_CFG1,PFC_CFG0] to 01, set Op Config [GPOUT_INT] to 0, and set Op Config [BAT_FN] to 0, in my opinion , the GPOUT pin has two functions: one is generating 0 or 1 signal based on the cell temp during charging as explained in table 5-9 in the TRM; two is following the status of the Flags( ) [SOC1] bit. Based on above assumptions, my question is how do I figure out if the state of GPOUT pin indicates over temp or the state of SOC. Or is my understanding of this incorrect? Does the GPOUT pin just indicate one function?