Hi dear,
I have to design an isolated dc-dc converter with input voltage range 18V - 36V and output 24V 3A with a switching frequency of 530KHz and size should be around 1/8 brick. I am buying the LM3481-FLYBACKEVM board.
I am not a power engineer therefore I need some advice regarding design parameters, selection of small size transformer and opto-coupler. It will be nice if you could provide some reference material and part manufacturers for transformer. Also, if you could some simulation software and design example.
Kind regards
Mohsin