I've been planning to use a TPS650532 for generating power supplies for my custom board. I want to feed all peripherals separately to minimize interferences. The system has USB, Bluetooth, 802.15.4 radio module and an external A/D converter chip.The TPS650532 provides two DC/DC converters and three LDO regulators, so it could meet my needs nicely (the fifth output would be for the OMAP itself).
Are there any better suggestions for powering a system like this, or other matters to be taken into consideration?
Thanks,
Harri Siirtola/Tech. Research Centre of Finland
Edit: Oops, should have posted this on the power management board. There seems to be no way of deleting or moving it myself, please move if needed...