Hi,
TPS53667 has "READ_IOUT" register and "IMON" pin.
When TPS53667 is used with CSD95490, current information is communicated from CSD95490.
Where is the measurement point of READ_IOUT?
Also, I do not understand the measurement point for IMON.
It seems that the output current is monitored by the analog current output from the IMON pin and the VMON obtained by RIMON,
but where is the current output from the IMON pin determined by the information from?
Best regards,
Yuto Sakai