Other Parts Discussed in Thread: BQSTUDIO, BQ24192
Hi, Ti engineers:
I'm using the bq27531 fuel gauge + bq24192 Charger application, communication is done through bqstudio(V1.3.80) + EV2300(V3.1m).(communication tested well).
According to the User's Guide of bq27531,I set the [DEFAULT_OVRD] bit and [BYPASS] bit true in Charger Option; and modify the Reg xx Default values in Charger Info by bqstudio, store them in the Data Flash of bq27531.
After that, I remove and insert the battery, and check the register values ,they are still RESET values; apparently, the bq27531 did not override them to the modified default values that are stored in the Data Flash as expected.
How can I override the charger register values automatically by 27531 Data Flash?