This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS568215: L and Cout component value

Part Number: TPS568215


TPS568215 has recommended components value table (Table 5).

Is the Cout min and max value effective capacitance value? And min value is requirement for stable operation? or transient response? Can we use lower Cout when we require fast transient response?

I think the components value not in list can also be used. Do you have any concern if we use the value not in list?

For example, when we use 1uH for 1Vout and 3.3Vout circuit, does Cout(min) value become lower with 1Vout circuit and become higher with 3.3Vout circuit?

I think there is no problem if "L x Cout " is same value.

Best Regards,
Kohei Sasaki