Hello
I use the LM5166 as a powersupply for a gate driver and use it in the following configuration:
- Mode: PFM
- Input voltage: ~46V
- Output voltage: 20V
- Laod max: 2W (100mA) ... coosen currrent limit resistor (open resistor) ==> peak current 440 ... 560mA (average >=220mA)
- EN-pin: turn on at 35V
- choke: 47uH
The problem I have with this is the following:
- When I have a switched load (swiched FET or equivalent) the LM5166 turns of after some time and doesn't turn on till I do a powercycle.
- Change of the layout for the output capacitor and the FB solved the problem for me on my bench but not it the actual environment the controller should be used.
- It should not be caused by thermal shutdown for the following reasons:
- Using a heatgun to increase the temperature didn't result in this behaviour
- Measurements with a thermal camera show, the the area stays rather cool
- It should not be cause by disabling the enable pin for the following reasons:
- PGOOD stays high for to long after the controller shuts down (about 50us)
- The same circuit the disables the enable pin also discharges the outpuit, but this doesn't happen.
So my question is: What reason can teh controller have to shut down suddenly and not come back?
Best Regards
Christoph