This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: LM5122 Shutdown Issue

Part Number: LM5122

I have a design using the LM5122 for a boost converter to convert 12V to 19V at 5A out. When the output current gets above about 4.1 or 4.2 amps, the output drops from 19V to about 11, and the LO signal will turn off and on at about 1 second intervals. This does not seem to be a thermal shutdown as the VCC output stays on solid.

What else would cause this behavior?

The schematic below is based on a Webench design.....